SPRUJF1 November 2024 AM2612
ADVANCE INFORMATION
The AM261x LaunchPad has a I2C based 1Mbit EEPROM (CAT24M01WI-GT3) to store board configuration details. The Board ID EEPROM is connected to the I2C1 interface of the AM261x SoC. The default I2C address of the EEPROM is set to 0x51 by pulling up the address pin A0 and pulling down the address pins A1 and A2 to ground. The Write Protect pin for the EEPROM is by default pulled down to ground and therefore Write Protect is disabled.