SPRZ375L October 2012 – June 2020 F28M36H33B2 , F28M36H53B2 , F28M36P53C2 , F28M36P63C2
This document describes the silicon updates to the functional specifications for the F28M36x microcontrollers (MCUs).
The updates are applicable to:
To designate the stages in the product development cycle, TI assigns prefixes to the part numbers of all Concerto MCU devices and support tools. Each Concerto MCU commercial family member has one of three prefixes: x, p, or no prefix (for example, xF28M36P63C2ZWTT). Texas Instruments recommends two of three possible prefix designators for its support tools: TMDX and TMDS. These prefixes represent evolutionary stages of product development from engineering prototypes (with prefix x/TMDX) through fully qualified production devices/tools (no prefix/TMDS).
xF28M36... | Experimental device that is not necessarily representative of the final device's electrical specifications | |
pF28M36... | Final silicon die that conforms to the device's electrical specifications but has not completed quality and reliability verification | |
F28M36... | Fully qualified production device |
Support tool development evolutionary flow:
TMDX | Development-support product that has not yet completed Texas Instruments internal qualification testing | |
TMDS | Fully qualified development-support product |
Devices with prefix x or p and TMDX development-support tools are shipped against the following disclaimer:
"Developmental product is intended for internal evaluation purposes."
Production devices and TMDS development-support tools have been characterized fully, and the quality and reliability of the device have been demonstrated fully. TI's standard warranty applies.
Predictions show that prototype devices with prefix of x or p have a greater failure rate than the standard production devices. Texas Instruments recommends that these devices not be used in any production system because their expected end-use failure rate still is undefined. Only qualified production devices are to be used.
TI device nomenclature also includes a suffix with the device family name. This suffix indicates the package type (for example, ZWT) and temperature range (for example, T).
Figure 1 provides an example of the Concerto device markings and defines each of the markings. The device revision can be determined by the symbols marked on the top of the package as shown in Figure 1. Some prototype devices may have markings different from those illustrated. Figure 2 shows an example of the device nomenclature.
PACKAGE MARKING CODE | SILICON REVISION | REVISION ID ADDRESS | REVISION ID(1) | COMMENTS |
---|---|---|---|---|
Blank | 0 | Arm®Cortex®-M3: 0x400F E000
C28x: 0x0883 |
0x0000 | Available as an experimental device. |
A | A | Arm Cortex-M3: 0x400F E000
C28x: 0x0883 |
0x0001 | Available as an experimental device and as a qualified production device. |
B | B | Arm Cortex-M3: 0x400F E000
C28x: 0x0883 |
0x0001 | Available as an experimental device and as a qualified production device. |
E | E | Arm Cortex-M3: 0x400F E000
C28x: 0x0883 |
0x0005 | Available as an experimental device and as a qualified production device. |
F | F | Arm Cortex-M3: 0x400F E000
C28x: 0x0883 |
0x0005 | Available as an experimental device and as a qualified production device. |