SPRZ488E March   2022  – May 2024 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
  3. 2Silicon Usage Notes
    1.     i2324
    2.     i2348
    3.     i2364
  4. 3Silicon Advisories
    1.     i2310
    2.     i2311
    3.     i2313
    4.     i2329
    5.     i2345
    6.     i2346
    7.     i2347
    8.     i2349
    9.     i2350
    10.     i2352
    11.     i2353
    12.     i2354
    13.     i2355
    14.     i2356
    15.     i2357
    16.     i2358
    17.     i2359
    18.     i2374
    19.     i2375
    20.     i2386
    21.     i2392
    22.     i2393
    23.     i2394
    24.     i2395
    25.     i2401
    26.     i2402
    27.     i2403
    28.     i2404
    29.     i2405
    30.     i2427
    31.     i2428
    32.     i2433
    33.     i2438
    34.     i2439
  5.   Trademarks
  6. 4Revision History

i2359

CONTROLSS-CMPSS:Prescaler counter behavior different from spec when DACSOURCE is made 0 or reconfigured as 1

Details:

While the prescaler is running, if we make DACSOURCE = 0 the prescale counter will not reset, if the enable condition is LOW the value stays, and when the DACSOURCE is again configured as 1 the counter starts from the previous value which was retained. This bug is present only when DACSOURCE is configured during the prescale counter running.

Workaround(s):

Issue a soft reset between DACSOURCE configuration which is not a dynamic configuration.