SPRZ488E March   2022  – May 2024 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
  3. 2Silicon Usage Notes
    1.     i2324
    2.     i2348
    3.     i2364
  4. 3Silicon Advisories
    1.     i2310
    2.     i2311
    3.     i2313
    4.     i2329
    5.     i2345
    6.     i2346
    7.     i2347
    8.     i2349
    9.     i2350
    10.     i2352
    11.     i2353
    12.     i2354
    13.     i2355
    14.     i2356
    15.     i2357
    16.     i2358
    17.     i2359
    18.     i2374
    19.     i2375
    20.     i2386
    21.     i2392
    22.     i2393
    23.     i2394
    24.     i2395
    25.     i2401
    26.     i2402
    27.     i2403
    28.     i2404
    29.     i2405
    30.     i2427
    31.     i2428
    32.     i2433
    33.     i2438
    34.     i2439
  5.   Trademarks
  6. 4Revision History

i2350

McSPI: McSPI data transfer using EDMA in ‘ABSYNC’ mode stops after 32 bits transfer

Details:

When EDMA is programmed to transfer more than 32 bits of data in to McSPI Tx FIFO (32 Bytes), it stops working after transferring only first 32 bits data in to the FIFO.

This issue is observed only in “ABSYNC” mode of EDMA where the EDMA is configured such that transfer size is more than 32 bits.

When the issue happens the EDMA neither transferring the data and completing it nor raising any error as vbusp_sdone signal is not getting generated by McSPI for transaction from EDMA.

SPI RX mode is not affected this issue.

Workaround(s):

Option1: Use ASYNC mode of EDMA for McSPI TX operation

Option2: Use acnt=4, bcnt=1, ccnt=1 if ABSYNC mode is used for McSPI TX operation