SPRZ491D december 2020 – june 2023 DRA821U , DRA821U-Q1
Table 1-1 shows the module(s) that are affected by each usage note.
MODULE | USAGE NOTE |
---|---|
N/A |
Table 1-2 shows the module(s) that are affected by each advisory.
MODULE | ADVISORY | SILICON REVISIONS AFFECTED | |
---|---|---|---|
SR 1.0 | SR 2.0 | ||
ADC | i2151 — ADC: Debounce time control register | YES | YES |
Boot | i2307 — Boot: ROM does not properly select OSPI clocking modes based on BOOTMODE | YES | YES |
i2360 — Boot: Ethernet RMII Boot Mode is not supported | YES | YES | |
i2361 — Boot: SPI and xSPI BOOTMODE Pin Mapping changes for SR2.0 | NO | YES | |
i2366 — Boot: ROM does not comprehend specific JEDEC SFDP features for 8D-8D-8D operation | YES | YES | |
i2371 — Boot: ROM code may hang in UART boot mode during data transfer | YES | YES | |
i2372 — Boot: ROM doesn't support select multi-plane addressing schemes in Serial NAND boot | NO | YES | |
CBASS | i2207 — CBASS: Command Arbitration Blocking | YES | YES |
i2235 — CBASS Null Error Interrupt Not Masked By Enable Register | YES | YES | |
CC | i2221 — CC: Invasive and Non-Invasive debug enable settings are reset by MCU_RESETz | YES | YES |
i2222 — Compute Cluster: A72 Corepac unable to be powered down | YES | YES | |
CP | i2283 — Restrictions on how CP Tracer Debug Probes can be used | YES | YES |
CPSW | i2184 — CPSW: IET express traffic policing issue | YES | YES |
i2185 — CPSW: Policer color marking issue | YES | YES | |
i2208 — CPSW: ALE IET Express Packet Drops | YES | YES | |
DCC | i2209 — DCC: Incorrect clock selection | YES | NO |
DDR | i2157 — DDR: Controller anomaly in setting wakeup time for low power states | YES | YES |
i2159 — DDR: VRCG high current mode must be used during LPDDR4 CBT | YES | YES | |
i2160 — DDR: Valid VRef Range Must be Defined During LPDDR4 Command Bus Training | YES | YES | |
i2166 — DDR: Entry and exit to/from Deep Sleep low-power state can cause PHY internal clock misalignment | YES | YES | |
i2182 — DDR: Dual-rank non-power-of-2 density not supported with row-cs-bank-col address mapping | YES | YES | |
i2186 — DDR rate limited to 2666 MT/s 1333 MHz clock | YES | NO | |
i2232 — DDR: Controller postpones more than allowed refreshes after frequency change | YES | YES | |
i2244 — DDR: Valid stop value must be defined for write DQ VREF training | YES | YES | |
i2274 — DDR: Including DDR in BSCAN causes current alarm on the DDR supply | YES | NO | |
DMSC | i2245 — DMSC: Firewall Region requires specific configuration | YES | YES |
i2275 — DMSC Secure Boot ROM: Potential Secure Boot vulnerability with explicit EC curve parameters in X.509 certificate | YES | NO | |
ECC AGGR | i2049 — ECC AGGR: Potential IP Clockstop/reset sequence hang due to pending ECC Aggregator interrupts | YES | YES |
I3C | i2197 — I3C: Slave mode is not supported | YES | YES |
i2205 — I3C Command fetched during pending IBI is not properly processed in some cases | YES | YES | |
i2216 — I3C: Command execution may fail during slave-initiated IBI address byte reception | YES | YES | |
IA | i2196 — IA: Potential deadlock scenarios in IA | YES | YES |
JTAG | i2228 — JTAG: TAP used by Debuggers may be inaccessible if TRSTn device pin is never asserted | YES | NO |
MCAN | i2278 — MCAN: Message Transmit order not guaranteed from dedicated Tx Buffers configured with same Message ID | YES | YES |
i2279 — MCAN: Specification Update for dedicated Tx Buffers and Tx Queues configured with same Message ID | YES | YES | |
MCU | i2217 — Recommended POST selection via MCU_BOOTMODE[09:08] | YES | NO |
MDIO | i2329 — MDIO: MDIO interface corruption (CPSW and PRU-ICSS) | YES | YES |
MMCSD | i2312 — MMCSD: HS200 and SDR104 Command Timeout Window Too Small | YES | YES |
MSMC | i2116 — MSMC: Set-hazarding logic withholding RT access waiting on NRT access completion | YES | YES |
i2187 — MSMC: Cache Resize to 0 Refreshes Tags instead of Updating them | YES | YES | |
i2201 — MSMC: Incorrect Parity Detect on bytecount | YES | NO | |
OSPI | i2189 — OSPI: Controller PHY Tuning Algorithm | YES | YES |
i2249 — OSPI: Internal PHY Loopback and Internal Pad Loopback clocking modes with DDR timing inoperable | YES | YES | |
i2351 — OSPI: Controller does not support Continuous Read mode with NAND Flash | YES | YES | |
i2383 — OSPI: 2-byte address is not supported in PHY DDR mode | YES | YES | |
PCIe | i2183 — PCIe: Link up failure when unused lanes are not assigned to PCIe Controller | YES | YES |
i2237 — PCIe: SerDes Reference Clock Output does not comply to Vcross, Rise-Fall Matching, and Edge Rate limits | YES | NO | |
i2241 — PCIe: The SerDes PCIe Reference Clock Output can exceed the 5.0 GT/s Data Rate RMS jitter limit | YES | NO | |
i2242 — PCIe: The 4-L SerDes PCIe Reference Clock Output is temporarily disabled while changing Data Rates | YES | YES | |
i2243 — PCIe: Timing requirement for disabling output refclk during L1.2 substate is not met | YES | YES | |
i2246 — PCIe: Automatic compliance entry fails when unused SERDES lanes are not assigned to PCIe Controller | YES | YES | |
i2326 — PCIe: MAIN_PLLx operating in fractional mode, which is required for enabling SSC, is not compliant with PCIe Refclk jitter limits | YES | YES | |
POK | i2277 — POK: De-Glitch (filter) is based upon only two samples | YES | NO |
PRG | i2253 — PRG: CTRL_MMR STAT registers are unreliable indicators of POK threshold failure | YES | YES |
PSIL | i2137 — Clock stop operation can result in undefined behavior | YES | YES |
R5FSS | i2161 — R5FSS: Debugger cannot access VIM module while it is active | YES | NO |
i2227 — R5FSS: Error interrupt CCM_COMPARE_STAT_PULSE_INTR incorrectly driven | YES | YES | |
RAT | i2062 — RAT: Error Interrupt Triggered Even When Error Logging Disable Is Set | YES | YES |
RINGACC | i2177 — RINGACC: The ring accelerator’s debug transaction trace stream can be corrupted by certain ring access sequences | YES | YES |
ROM Code | i2306 — ROM Code: Need to turn off internal termination resistors in SERDES | YES | NO |
SGMII | i2362 — 10-100M SGMII: Marvell PHY does not ignore the preamble byte resulting in link failure | YES | YES |
STOG | i2123 — STOG: Timed Out Emulation Debug write responses from the Slave Gasket always return Success | YES | YES |
i2126 — STOG: Error miscounting when there are two concurrent timeouts or two concurrent unexpected responses | YES | YES | |
i2127 — STOG: SRC side write data bus hang when a write command timeout occurs the same cycle as last acceptance on DST side | YES | YES | |
UDMA | i2146 — UDMA: Force teardown bitfield readback is masked in realtime TX/RX registers | YES | YES |
i2320 — UDMA, UDMAP: Descriptors and TRs required to be returned unfragmented | YES | YES | |
UDMAP | i2163 — UDMAP: UDMA transfers with ICNTs and/or src/dst addr NOT aligned to 64B fail when used in "event trigger" mode | YES | YES |
i2234 — UDMA: TR15 hangs if ICNT0 is less than 64 bytes | YES | YES | |
USART | i2310 — USART: Erroneous clear/trigger of timeout interrupt | YES | YES |
i2311 — USART: Spurious DMA Interrupts | YES | YES | |
USB | i2091 — 2.0 PHY hangs if received signal amplitude crosses squelch threshold multiple times within the same packet | YES | YES |
i2134 — USB: 2.0 compliance receive sensitivity test limitation | YES | YES | |
xSPI | i2257 — xSPI boot mode redundant image boot failure | YES | NO |