SPRZ536B September   2022  – July 2024 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1

 

  1.   1
  2. 1Modules Affected
  3. 2Nomenclature, Package Symbolization, and Revision Identification
    1. 2.1 Device and Development-Support Tool Nomenclature
    2. 2.2 Devices Supported
    3. 2.3 Package Symbolization and Revision Identification
  4. 3Silicon Revision 1.0 Usage Notes and Advisories
    1. 3.1 Silicon Revision 1.0 Usage Notes
      1.      i2134
    2. 3.2 Silicon Revision 1.0 Advisories
      1.      i2049
      2.      i2062
      3.      i2063
      4.      i2064
      5.      i2065
      6.      i2079
      7.      i2097
      8.      i2102
      9.      i2103
      10.      i2120
      11.      i2134
      12.      i2137
      13.      i2146
      14.      i2157
      15.      i2159
      16.      i2160
      17.      i2161
      18.      i2163
      19.      i2166
      20.      i2177
      21.      i2189
      22.      i2190
      23.      i2196
      24.      i2197
      25.      i2205
      26.      i2215
      27.      i2216
      28.      i2219
      29.      i2232
      30.      i2234
      31.      i2242
      32.      i2244
      33.      i2249
      34.      i2253
      35.      i2271
      36.      i2272
      37.      i2278
      38.      i2279
      39.      i2310
      40.      i2311
      41.      i2312
      42.      i2320
      43.      i2326
      44.      i2351
      45.      i2362
      46.      i2366
      47.      i2371
      48.      i2372
      49.      i2378
      50.      i2381
      51.      i2383
      52.      i2399
      53.      i2401
      54.      i2409
      55.      i2414
      56.      i2419
      57.      i2422
      58.      i2435
      59.      i2437
  5.   Trademarks
  6.   Revision History

i2120


C71x: SE Hangs on Non-Parity Error Detection in Transposed Streams With LEZR

Details:

The C71x Streaming Engine's (SE) pipeline for returning formatted data and return report internal error information is always monitoring the tags for the data that it is working on. When an error is detected for a line of data used to format data back to the CPU, all fetching side execution for queuing up commands to go to UMC, uTLB, and the formatting pipeline back to CPU is halted.

In general operation, the only tags monitored for errors are the ones being used for the current command. For transposed mode, this is all tags touched by the current array column. A gap in suppressing internal tag monitoring causes the formatting pipeline to monitor tags that it is not currently working on while creating zero vectors for the LEZR feature. If the SE's fetching side encounters and records an error for a future column, the formatting side may notice it and halt the fetching side before the command for that column has been committed for formatting.

Errors are only reported back to the CPU for commands that are internally committed for formatting, thus halting internal execution before committing the column results in no error being reported to the CPU. Because the SE has halted fetching operations without reporting an error, the CPU proceeds to hang, waiting for either return data or an error from the SE, until an unrelated external event or interrupt occurs.

Workaround(s):

The only 100% workaround is to not use stream templates with both LEZR and transposed mode enabled.