SPRZ572A April 2024 – September 2024 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SJ-Q1
Flash: Single-Bit ECC Error Interrupt is Not Generated
0, A
If the single-bit ECC error threshold is configured as 0, the single-bit error interrupt is not generated when there is a single-bit error.
Set the error threshold bit field (FLASH_ECC_REGS ERR_THRESHOLD.ERR_THRESHOLD field) to a value greater than or equal to 1. Note that the default value of the threshold bit field is 0.