CONTROLSS |
i2352 — CONTROLSS-SDFM: Dynamically
Changing Threshold Settings (LLT, HLT), Filter Type, or COSR
Settings Will Trigger Spurious Comparator Events |
YES |
CONTROLSS |
i2353 — CONTROLSS-SDFM: Dynamically
Changing Data Filter Settings (Such as Filter Type or DOSR) Will
Trigger Spurious Data Acknowledge Events |
YES |
CONTROLSS |
i2354 — CONTROLSS-SDFM: Two Back-to-Back
Writes to SDCPARMx Register Bit Fields CEVT1SEL, CEVT2SEL, and HZEN
Within Three SD-Modulator Clock Cycles can Corrupt SDFM State
Machine, Resulting in Spurious Comparator Events |
YES |
CONTROLSS |
i2356 — CONTROLSS-ADC: Interrupts may Stop
if INTxCONT (Continue-to-Interrupt Mode) is not Set |
YES |
CONTROLSS |
i2357 — CONTROLSS-ePWM: An ePWM Glitch can
Occur if a Trip Remains Active at the End of the Blanking
Window |
YES |
CONTROLSS |
i2358 — CONTROLSS-ePWM: Trip Events Will
Not be Filtered by the Blanking Window for the First 3 Cycles After
the Start of a Blanking |
YES |
CONTROLSS |
i2359 — CONTROLSS-CMPSS:Prescaler counter
behavior different from spec when DACSOURCE is made 0 or
reconfigured as 1 |
YES |
CPSW |
i2345 — CPSW: Ethernet Packet corruption
occurs if CPDMA fetches a packet which spans across memory
banks |
YES |
UART |
i2310 — USART: Erroneous triggering of
timeout interrupt |
YES |
UART |
i2311 — USART: Spurious DMA
Interrupts |
YES |
DTHE |
i2428 — AES in DTHE generates extra dma request for data_in at the end
of GCM encrypt |
YES |
SEC |
i2427 — RAM SEC can cause Spurious RAM writes resulting in L2 &
MBOX memory corruption |
YES |
USB |
i2412 — USB can not generate interrupt upon DMA read/Write Access error |
YES |
TCM |
i2411 — 128 Bytes burst access is not supported for TCM |
YES |
OSPI |
i2383 — OSPI: 2-byte address is not supported in PHY DDR mode |
YES |
PBIST |
i2374 — PBIST fails if clock frequency of R5SS_CORE_CLK is not same as
R5FSS_CLK_SELECTED frequency |
YES |
OSPI |
i2351 — OSPI: Direct Access Controller (DAC) does not support
Continuous Read mode with NAND Flash |
YES |
OSPI |
i2189 — OSPI: Controller PHY Tuning Algorithm |
YES |
CPSW |
i2440 - CPSW: Host to Ethernet Timestamp Sequence ID issue |
YES |
CPSW |
i2439 - CPSW: Host to Ethernet Timestamp Accuracy Issue |
YES |
ICSS |
i2433 - ICSS: Reading the 64-bit IEP timer does not have a lock MSW
logic when LSW is read |
YES |