SPRZ578 December 2024 AM2754-Q1
C71x: SE returning incorrect data when non-aligned transposed stream crosses AM1 circular buffer boundary
When AM1 refers to a larger circular buffer size than AM0, SE can reuse the wrong 64B line of data during non-aligned transposed streams. This occurs when one of the rows being transposed crosses the AM1 circular buffer boundary, but not the AM0 boundary.
Have the transposed stream either be fully aligned, meaning that the start address and all scaled DIM values be multiples of 64B, or to not configure AM1 to be a larger circular addressing buffers size than AM0.