SPRZ578 December   2024 AM2754-Q1

 

  1.   1
  2.   Abstract
  3. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  4. 2Silicon Revision Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2284
      2.      i2351
      3.      i2424
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2120
      4.      i2137
      5.      i2189
      6.      i2196
      7.      i2199
      8.      i2249
      9.      i2253
      10.      i2278
      11.      i2279
      12.      i2310
      13.      i2311
      14.      i2312
      15.      i2383
      16.      i2401
      17.      i2427
      18.      i2431
      19.      i2435
      20.      i2436
      21.      i2438
      22.      i2455
  5. 3Trademarks
  6. 4Revision History

i2310

USART: Erroneous clear/trigger of timeout interrupt

Details:

The USART may erroneously clear or trigger the timeout interrupt when RHR/MSR/LSR registers are read.

Workaround(s):

For CPU use-case.

  • If the timeout interrupt is erroneously cleared:
    • This is Valid since the pending data inside the FIFO will retrigger the timeout interrupt
  • If timeout interrupt is erroneously set, and the FIFO is empty, use the following SW workaround to clear the interrupt:
    • Set a high value of timeout counter in TIMEOUTH and TIMEOUTL registers
    • Set EFR2 bit 6 to 1 to change timeout mode to periodic
    • Read the IIR register to clear the interrupt
    • Set EFR2 bit 6 back to 0 to change timeout mode back to the original mode

For DMA use-case.

  • If timeout interrupt is erroneously cleared:
    • This is valid since the next periodic event will retrigger the timeout interrupt
    • User must ensure that RX timeout behavior is in periodic mode by setting EFR2 bit6 to 1
  • If timeout interrupt is erroneously set:
    • This will cause DMA to be torn down by the SW driver
    • Valid since next incoming data will cause SW to setup DMA again