SSZTB54 June 2016 TPS65023-Q1 , TPS65321-Q1
Martin Asch
In part 1 of this series, I used an example application that required a high current at the higher-voltage rail and a low current at the lower-voltage rail. But what if the situation was reversed and only a small current is needed at the higher-voltage rail while most of the system load is supplied through the lower voltage rail?
A common requirement for automotive systems is to keep the communication, more often than not handled by a controller area network (CAN) transceiver running at 5V, alive even when the rest of the system is shut off – the perfect scenario for a standby low-dropout regulator (LDO) supplying a stable 5V rail. The other components of the system typically run at the same or a lower voltage but require a much higher current, such as a microcontroller, memory, light-emitting diode (LED) driver, motor driver, additional interfaces or point-of-load voltage regulators.
In this installment of my two-part series, the application example is an automotive head-up display (HUD). The HUD’s power tree consists of two rails with different current requirements. The 5V rail needs a maximum of 100mA to supply an always-on CAN transceiver. All other loads are powered by the 3.3V rail. A low-voltage power-management integrated circuit (IC) running off the 3.3V rail and drawing up to 2A of current supplies the microprocessor and double data rate (DDR) memory as well as the rest of the system, as shown in Figure 1.
HUD units today often solve these requirements by utilizing a discrete buck and LDO solution, but the available space on top of the car dashboard is extremely limited. Every inch of saved board space directly benefits the passengers and increases the interior space of the car. Size really matters. By integrating the discrete solution into one chip and addressing the power tree with a combined step-down converter and LDO regulator, the solution size can be reduced by more than 25%.
When using an integrated solution, you don’t need to sacrifice the benefits of a discrete implementation: Both the buck and LDO can activate separately and are capable of connecting straight to the battery, allowing for completely independent output voltages and maximum flexibility when supplying the power rails.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated