SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
Table 5-9 shows that the interrupts with vector number from 16 to 49 are sourced by the events routed in the MCU event fabric to the system CPU. The event fabric routes all level interrupt events to the system CPU. The event/interrupt called AON programmable 0 can be configured in the AON event fabric. EVENT:CPUIRQSEL29 is a read-only register for routing within the MCU event fabric and cannot be configured, but the input event within the AON event fabric going to this line can be configured. One dynamic event/interrupt called Dynamic Programmable Event has the valid selections that are shown in Table 5-9. The EVENT:CPUIRQSEL29 register is used to configure the input (see Section 5.8.2).
See the EVENT:CPUIRQSEL30 register in see Section 5.8.2.