SWRA446 February   2015 CC1310 , CC1310 , CC2620 , CC2620 , CC2630 , CC2630 , CC2640 , CC2640 , CC2640R2F , CC2640R2F , CC2640R2F-Q1 , CC2640R2F-Q1 , CC2650 , CC2650 , CC2650MODA , CC2650MODA

 

  1.   Using GCC/GDB With SimpleLink CC26xx/CC13xx
    1.     Trademarks
    2. 1 Introduction
    3. 2 Prerequisites
      1. 2.1 Platforms
      2. 2.2 Hardware
      3. 2.3 Software
    4. 3 Hardware Setup
    5. 4 Software Installation Instructions
      1. 4.1 Java Runtime Environment
      2. 4.2 Eclipse IDE (Windows)
      3. 4.3 Eclipse IDE (Linux)
      4. 4.4 GNU Toolchain (Windows)
      5. 4.5 GNU Toolchain (Linux)
      6. 4.6 Build Tools for Windows
      7. 4.7 TI Emupack and GDB Server (Windows)
      8. 4.8 Flash Programmer (Windows)
      9. 4.9 Flash Programmer (Linux)
    6. 5 Build the Software Example
      1. 5.1 Import Example Project Into the IDE
      2. 5.2 Build the Software Example
    7. 6 Load Binary Image to Target
      1. 6.1 Configure Flash Programmer Tool (Windows)
      2. 6.2 Configure Flash Programmer Tool (Linux)
      3. 6.3 Load the Image to Target (Windows)
      4. 6.4 Load the Image to Target (Linux)
    8. 7 Debug the Software Example
      1. 7.1 Launch the GDB Server (Windows)
      2. 7.2 Launch the GDB Server (Linux)
      3. 7.3 Configure Eclipse Debugger
      4. 7.4 Running the Software Example From Debugger
    9. 8 References
  2. AMakefile
    1. A.1 Makedefs
    2. A.2 Makefile
  3. BLinker and Startup Files
    1. B.1 Linker File
    2. B.2 Startup Files

Build Tools for Windows

If your development platform is Windows, an additional command line program, ‘make’, is required by the Eclipse external builder. One choice is to download the MinGW tool. Perform the following steps for installation:

  1. Download the MinGW setup tool from http://www.mingw.org/.
  2. Run the Setup. Choose default installation directory.
  3. Click Continue when the setup is finished to open the installation manager.
  4. In the Installation Manager, mark ‘All Packages’ in the left panel. Click on the checkboxes for the packages called mingw32-make and mingw32-gcc and select ‘mark for installation’.
  5. installing_mingw_windows.gifFigure 7. Installing MinGW (Windows)
  6. Choose Installation → Apply Changes and click the ‘Apply’ button.
  7. installing_mingw_windows_2.gifFigure 8. Installing MinGW (Windows)
  8. Finally, add the installation path (default: C:\MinGW\bin) to your environment variables. This is done by going to Control Panel → System and Security → System → Advanced system settings. Append the installation path to the PATH variable.