SWRA446 February 2015 CC1310 , CC1310 , CC2620 , CC2620 , CC2630 , CC2630 , CC2640 , CC2640 , CC2640R2F , CC2640R2F , CC2640R2F-Q1 , CC2640R2F-Q1 , CC2650 , CC2650 , CC2650MODA , CC2650MODA
For Windows, the binary image that was generated in the previous section will be loaded to the target using the SmartRF flash Programmer 2 tool.
Load the binary image to the target by running the Flash Programmer tool: Run → External Tools → External Tools Configurations ... . Select Flash program under 'Program' in the left side panel and click 'Run'. The console output should be similar to the output shown in Figure 18.