SWRA465A August   2014  – July 2015 CC2530 , CC2530 , CC2530-RF4CE , CC2530-RF4CE , CC2592 , CC2592

 

  1.   Using CC2592 Front End With CC2530
    1.     Trademarks
    2. Introduction
    3. Acronyms Used in This Documents
    4. Absolute Maximum Ratings
    5. Electrical Specifications
      1. 4.1 Operating Conditions
      2. 4.2 Current Consumption
      3. 4.3 Receive Parameters
      4. 4.4 Received Signal Strength Indicator (RSSI)
      5. 4.5 Transmit Parameters
      6. 4.6 Output Power Programming
      7. 4.7 Typical Performance Curves
      8. 4.8 IEEE - Transmit Power Spectral Density (PSD) Mask
    6. Application Circuit
      1. 5.1 Power Decoupling
      2. 5.2 Input /Output Matching and Filtering
      3. 5.3 Bias Resistor
      4. 5.4 Antenna Considerations
    7. PCB Layout Considerations
      1. 6.1 The Gain of the CC2592
    8. Regulatory Requirements
      1. 7.1 Compliance of FCC Part 15.247 When Using the CC2530 With the CC2592
    9. Controlling the CC2592
    10. Integrating CC2592 With Z-Stack and TIMAC
    11. 10 References
  2.   A Marker - Delta Method
    1.     A.1
  3.   Revision History

  • Power Setting: 0xE5
  • Set the DUT in Modulated TX
  • Center Frequency: 2480 MHz
  • Span: 10 MHz
  • RBW VBW Detector Meas. Name Power Comments
    1 MHz 1 MHz Max Peak + Max Hold PEAK 18.9
    1 MHz 10 Hz Average + Max Hold AVERAGE 16.6 The power will be lower for AVERAGE than for PEAK
  • Choose a spectrum analyzer that encompasses both the peak of the fundamental emission and the band-edge emission under investigation (for example, 2483.5 MHz, edge in Figure 13).
  • band_edge_setupb.pngFigure 13. Band-Edge Setup
    RBW VBW Detector Meas. Name Power Comments
    1% of total span >= RBW (100 KHz) Max Peak + Max Hold TOP PEAK 13.0 RBW - never less than 30 kHz. Several sweeps in peak hold mode
    1% of total span >= RBW (100 KHz) Max Peak + Max Hold Band-Edge PEAK -33.0 RBW - never less than 30 kHz. Several sweeps in peak hold mode
    TOP PEAK - Band Edge PEAK -> DELTA 46.0 Delta will normally be > 40dB
  • Record the peak levels of the fundamental emission and the relevant band edge emission. The band edge peak is measured at the highest point to the right of the 2483.5 MHz line, which is typically on this line. However in some cases there may be a higher peak nearby. Observe the stored trace and measure the amplitude delta between the top peak of the fundamental and the peak of the band-edge emission.
  • Note a lower RBW, even as low as 30 KHz, may be required to see the band-edge peak.
  • When the DELTA value is calculated, use it to check how the PEAK and Average values are compared to their respective limits.
Math Power (dBm) Limits/Comments
PEAK - DELTA = -27.1 –21.2 dBm (74 dBuV/m)
AVERAGE - DELTA = -29.4 –41.2 dBm (54 dBuV/m)
BACK OFF = (-29.4) - (-41.2) = 11.8 Required back off on channel 26