4.1.2 Initializating TI-RTOS
For more information on the device initialization by TI-RTOS, see Figure 9.
- Make sure all code is compiled with the same version of driverlib— Ensure that the TI-RTOS implementation is built with the same version of driverlib as the rest of the application.
- Set standby disallow constraint pending LF clock qualifier disabling— TI-RTOS-specific code to ensure the application enters standby after the LF clock source selected in CCFG is selected and stable. Disable the LF clock qualifiers after selecting the LF clock source.