SWRA495K December 2015 – April 2024 CC1310 , CC1350 , CC2620 , CC2630 , CC2640 , CC2640R2F , CC2640R2F-Q1 , CC2642R-Q1 , CC2650 , CC2662R-Q1
ESR (equivalent series resistance) is a parameter of the crystal in the data sheet of the crystal. Negative resistance is a parameter of the complete oscillator circuit, including capacitor values, crystal parameters, and an on-chip circuit. To ensure best start-up of the crystal oscillator, the negative resistance magnitude must be at least 3 times greater than RN (see Equation 10 and Equation 11) during initial start up.
If the negative resistance magnitude is not 3× greater than ESR during initial start-up, the oscillator might not operate optimally or might fail to start in the presence of environmental changes or manufacturing variations in the crystal.