SWRA513C January 2020 – September 2020 CC3120 , CC3120MOD , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Once the provisioning process starts, it repeatedly switches between the configuration and confirmation stages until one of the following occurs.
When the provisioning process stops due to host request or after inactivity time-out expires, the device switches back to the role that was active when the provisioning process started. If the process stops because a profile was successfully confirmed, the device switches to the role defined by the host during the provisioning start command.
After provisioning successfully stops, the host receives a PROVISIONING_STOPPED status event. The event is sent after switching to the desired role is complete. When the host issues a provisioning stop command, it should wait for the PROVISIONING_STOPPED event before issuing additional commands.