SWRA513C January 2020 – September 2020 CC3120 , CC3120MOD , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Figure 8-7 shows a sequence diagram describing a successful provisioning process using the SmartConfig method while external configuration is enabled.
When Provisioning is started in APSC plus External configuration mode, and the user is using one of the internal provisioning methods (AP or SC), the device sends a reset request event to the host. The host should close all the sockets and activities of its external provisioning process, and restart the device. When the device is restarted, it continues to the confirmation stage and the internal provisioning process continues as usual.