SWRA513C January 2020 – September 2020 CC3120 , CC3120MOD , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
The SimpleLink Wi-Fi device is in AP role, simultaneously scanning for SmartConfig broadcasts. Users can either connect with an external device (such as a smartphone) to the SimpleLink AP, and add a profile through the HTTP/HTTPS server of the device, or add a profile using a SmartConfig-capable smartphone application. This configuration mode can also deliver the confirmation result to users if it was not successfully delivered during the confirmation stage.