SWRA513C January 2020 – September 2020 CC3120 , CC3120MOD , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
When feedback is delivered locally, the user’s smartphone provisioning app must connect to the same wireless network to which the SimpleLink Wi-Fi device is connected, and ask the HTTP server of the device for the confirmation result. To do so, the smartphone provisioning app must discover the new IP address the device acquired. After the SimpleLink Wi-Fi device successfully acquires an IP address, it advertises itself using broadcast and multicast packets, to enable the smartphone provisioning app to discover its address.