SWRA513C January 2020 – September 2020 CC3120 , CC3120MOD , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Figure 8-6 shows a sequence diagram describing a successful provisioning process using an external provisioning method WAC.
When Provisioning is started in APSC plus External configuration mode, the host can start sending commands to the networking subsystem only after the external configuration ready provisioning status event is received. When the host identifies that a user has started a provisioning process using the external configuration method, it should order the networking subsystem to stop the internal provisioning process. When the networking subsystem is stopped, the host can continue with its provisioning process.