SWRA640H December 2018 – May 2024 CC1310 , CC1312R , CC1314R10 , CC1350 , CC1352P , CC1352R , CC1354P10 , CC1354R10 , CC2620 , CC2630 , CC2640 , CC2640R2F , CC2640R2F-Q1 , CC2642R , CC2642R-Q1 , CC2650 , CC2652P , CC2652R , CC2652R7 , CC2652RB , CC2652RSIP , CC2674P10 , CC2674R10
This antenna design is based on LaunchPad-CC1352P-4 that uses the 433MHz to 930MHz and 2.4GHz BOM Tunable PCB Antenna. This BOM Tunable Antenna is fully documented 433 to 930-MHz and 2.4-GHz BOM Tunable PCB Antenna, application note.
In order to cover the frequency band 433 – 510MHz, an external component (LANT) is added to the antenna structure normally used for 863-928MHz and 2.4GHz. This is required to keep the antenna relatively small and to maintain a high efficiency. The LANT component extends the length of the antenna structure with the extra inductance added. It is difficult to cover the entire frequency band of 433 – 510MHz with just one BOM due to the wide bandwidth so the frequency range is divided up into the several regions. An additional antenna structure has also been added that also extends the length of the standard antenna, see Figure 5-7.
Value of LANT component for 433-510MHz operation:
Once the LANT component has been chosen then the matching procedure is similar as shown in the previous example. After the antenna matching process, the final values of the antenna match components can be fixed. As can be seen in Figure 5-8, the matching of 490MHz and 2.4GHz are both below VSWR 1.90 :1, which are good results.
Matching the antenna should be performed in the final casing of the product including all surrounding components such as batteries, displays, and so forth. Casing can affect the antenna’s resonance even if the material choice is plastic. The positioning of the antenna or body effects will also affect the antenna’s resonance. The antenna is always detuned by a shift downwards in frequency. Therefore, if there are two different environments for the antenna such as handheld and stand-alone on a wooden desk, then it is preferable to have the stand-alone resonance slightly higher so the antenna’s bandwidth can be utilized when detuned by body effects/metal objects, and so forth.