SWRA681 September   2020 CC3100 , CC3100MOD , CC3120 , CC3120MOD , CC3135 , CC3135MOD , CC3200 , CC3200MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2CE Conformity Test Requirements and Test Procedure for Wi-Fi Devices
    1. 2.1 Test Setup for Compliance Testing
    2. 2.2 Test Conditions
    3. 2.3 Test Configurations of the EUT
    4. 2.4 Configuring and Testing the EUT (Wi-Fi Device – CC3xxx)
      1. 2.4.1 Setting-Up the Country Code
      2. 2.4.2 Duty Cycle for Measurement of Tx Parameters
  5. 3Test Procedure for Compliance Testing - EN 300 328
    1. 3.1 Product Information as per Annex-E of EN 300 328
    2. 3.2 RF Output Power - EN 300 328
    3. 3.3 Power Spectral Density - EN 300 328
    4. 3.4 Occupied Channel Bandwidth (OCBW) - EN 300 328
    5. 3.5 Transmitter Unwanted Emissions in the OOB Domain - EN 300 328
    6. 3.6 Transmitter Unwanted Emissions in the Spurious Domain - EN 300 328
    7. 3.7 Adaptivity (Channel Access Mechanism) - EN 300 328
    8. 3.8 Receiver Spurious Emissions - EN 300 328
    9. 3.9 Receiver Blocking - EN 300 328
  6. 4Test Procedure for Compliance Testing for Wi-Fi Devices - EN 301 893
    1. 4.1  Product Information as per Annex-G of EN 301 893
    2. 4.2  Test Channels - EN 301 893
    3. 4.3  Nominal Center Frequencies - EN 301 893
    4. 4.4  Occupied Channel Bandwidth (OCBW) - EN 301 893
    5. 4.5  RF Output Power - EN 301 893
    6. 4.6  Power Spectral Density - EN 301 893
    7. 4.7  Tx Unwanted Emissions Outside the 5 GHz RLAN Band - EN 301 893
    8. 4.8  Tx Unwanted Emissions Within the 5 GHz RLAN Bands - EN 301 893
    9. 4.9  Receiver Spurious Emissions - EN 301 893
    10. 4.10 Receiver Blocking - EN 301 893
    11. 4.11 Adaptivity (Channel Access Mechanism) - EN 301 893
    12. 4.12 Dynamic Frequency Selection (DFS) - EN 301 893
    13. 4.13 User Access Restrictions - EN 301 893
  7. 5Test Procedure for Compliance Testing for Wi-Fi Devices - EN 301 489
    1. 5.1 Radiated Emissions – Enclosure Port - EN 301 489
    2. 5.2 Conducted Emissions – DC Power Input/Output Port - EN 301 489
    3. 5.3 RF Electromagnetic Field (80 MHz to 6000 MHz) - EN 301 489
    4. 5.4 Electrostatic Discharge - EN 301 489
  8. 6Test Procedure for Compliance Testing for Wi-Fi Devices – IEC 62368-1
    1. 6.1 General Requirements – IEC 62368-1
    2. 6.2 Electrically Caused Injury – IEC 62368-1
    3. 6.3 Electrically Caused Fire – IEC 62368-1
    4. 6.4 Injury Caused by Hazardous Substances – IEC 62368-1
    5. 6.5 Mechanically Caused injury – IEC 62368-1
    6. 6.6 Thermal Burn Injury – IEC 62368-1
    7. 6.7 Radiation – IEC 62368-1
  9. 7Test Assessment for Human Exposure Restrictions – EN 62311
  10. 8References

RF Electromagnetic Field (80 MHz to 6000 MHz) - EN 301 489

This test assesses the ability of the EUT to operate as intended in the presence of a radio frequency electromagnetic field disturbance. This test is applicable for radio equipment and associated ancillary equipment. This test is performed on a representative configuration of the radio equipment. For test requirements, see the RF Electromagnetic Field (80 MHz to 6000 MHz) - Enclosure Port section in CE Regulations for SRDs Operating in License-Free 2.4 GHz/5 GHz Bands [1].

The EUT is configured to its intended operational mode in the frequency band being investigated. The configuration and mode of operation used in the measurement are noted in the test report. The test method is in accordance with CENELEC EN 61000-4-3 [19], clauses 6, 7 and 8. The test results comply with the performance criteria for continuous phenomena shown in the Performance Criteria section in CE Regulations for SRDs Operating in License-Free 2.4 GHz/5 GHz Bands [1] and is recorded in the test report. The test procedure for RF Electromagnetic field measurement is described in the following steps:

  1. For test setup, see CENELEC EN 61000-4-3 [19], clauses 6, 7 and 8.
  2. For detailed test procedures, see CENELEC EN 61000-4-3 [19], clauses 6, 7 and 8.
  3. Switch ON the EUT and other test equipment.
  4. Use the Radio Testing Tool [9] to setup and configure the EUT. For setting and up configuring the EUT, see the Radio Testing Tool User's Guide [10].
  5. Open the Radio Testing Tool [9] and setup the link with the EUT by using the Setup tab.
  6. Open the Tx tab and set the transmission mode to “Continuous”.
  7. Configure the EUT to the desired parameters such as Channel/Frequency, Data Rate, Data Pattern, Power Level, and so forth).
  8. Click on “ Start Tx Testing”.
  9. If it requires use of the Companion device for link performance testing.
  10. Carry out the test as per the test method in CENELEC EN 61000-4-3 [19], clauses 6, 7 and 8.
  11. Repeat the above for other data rates/modulations and also other desired channels.
  12. The test results comply with the performance criteria for continuous phenomena shown in the Performance Criteria section in CE Regulations for SRDs Operating in License-Free 2.4 GHz/5 GHz Bands [1].