SWRA681 September   2020 CC3100 , CC3100MOD , CC3120 , CC3120MOD , CC3135 , CC3135MOD , CC3200 , CC3200MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2CE Conformity Test Requirements and Test Procedure for Wi-Fi Devices
    1. 2.1 Test Setup for Compliance Testing
    2. 2.2 Test Conditions
    3. 2.3 Test Configurations of the EUT
    4. 2.4 Configuring and Testing the EUT (Wi-Fi Device – CC3xxx)
      1. 2.4.1 Setting-Up the Country Code
      2. 2.4.2 Duty Cycle for Measurement of Tx Parameters
  5. 3Test Procedure for Compliance Testing - EN 300 328
    1. 3.1 Product Information as per Annex-E of EN 300 328
    2. 3.2 RF Output Power - EN 300 328
    3. 3.3 Power Spectral Density - EN 300 328
    4. 3.4 Occupied Channel Bandwidth (OCBW) - EN 300 328
    5. 3.5 Transmitter Unwanted Emissions in the OOB Domain - EN 300 328
    6. 3.6 Transmitter Unwanted Emissions in the Spurious Domain - EN 300 328
    7. 3.7 Adaptivity (Channel Access Mechanism) - EN 300 328
    8. 3.8 Receiver Spurious Emissions - EN 300 328
    9. 3.9 Receiver Blocking - EN 300 328
  6. 4Test Procedure for Compliance Testing for Wi-Fi Devices - EN 301 893
    1. 4.1  Product Information as per Annex-G of EN 301 893
    2. 4.2  Test Channels - EN 301 893
    3. 4.3  Nominal Center Frequencies - EN 301 893
    4. 4.4  Occupied Channel Bandwidth (OCBW) - EN 301 893
    5. 4.5  RF Output Power - EN 301 893
    6. 4.6  Power Spectral Density - EN 301 893
    7. 4.7  Tx Unwanted Emissions Outside the 5 GHz RLAN Band - EN 301 893
    8. 4.8  Tx Unwanted Emissions Within the 5 GHz RLAN Bands - EN 301 893
    9. 4.9  Receiver Spurious Emissions - EN 301 893
    10. 4.10 Receiver Blocking - EN 301 893
    11. 4.11 Adaptivity (Channel Access Mechanism) - EN 301 893
    12. 4.12 Dynamic Frequency Selection (DFS) - EN 301 893
    13. 4.13 User Access Restrictions - EN 301 893
  7. 5Test Procedure for Compliance Testing for Wi-Fi Devices - EN 301 489
    1. 5.1 Radiated Emissions – Enclosure Port - EN 301 489
    2. 5.2 Conducted Emissions – DC Power Input/Output Port - EN 301 489
    3. 5.3 RF Electromagnetic Field (80 MHz to 6000 MHz) - EN 301 489
    4. 5.4 Electrostatic Discharge - EN 301 489
  8. 6Test Procedure for Compliance Testing for Wi-Fi Devices – IEC 62368-1
    1. 6.1 General Requirements – IEC 62368-1
    2. 6.2 Electrically Caused Injury – IEC 62368-1
    3. 6.3 Electrically Caused Fire – IEC 62368-1
    4. 6.4 Injury Caused by Hazardous Substances – IEC 62368-1
    5. 6.5 Mechanically Caused injury – IEC 62368-1
    6. 6.6 Thermal Burn Injury – IEC 62368-1
    7. 6.7 Radiation – IEC 62368-1
  9. 7Test Assessment for Human Exposure Restrictions – EN 62311
  10. 8References

Test Channels - EN 301 893

Unless otherwise stated in the test procedure for individual tests in the following sub-sections, the channels are used for testing is shown in Table 4-1.

Table 4-1 Test Channels – EN 301 893 [4]
Test

Clause of EN301 893 ()

Test Channels

Lower Sub-Band (5150 MHz to 5350 MHz)

Higher Sub-Band 5470 MHz to 5725 MHz

5150 MHz to 5250 MHz 5250 MHz to 5350 MHz
Centre frequencies 5.4.2 C7 (see note 1) C8 (see note 1)

Occupied Channel

Bandwidth

5.4.3 C7 C8
Power, Power Density 5.4.4 C1 C2 C3, C4

Transmitter unwanted

emissions outside the

5 GHz RLAN bands

5.4.5 C7 (see note 1) C8 (see note 1)

Transmitter unwanted

emissions within the

5 GHz RLAN bands

5.4.6 C1 C2 C3, C4

Receiver spurious

emissions

5.4.7 C7 (see note 1) C8 (see note 1)
Transmit Power Control (TPC) 5.4.4 NA (see note 2) C2 (see note 1) C3, C4 (see note 1)

Dynamic Frequency

Selection (DFS)

5.4.8 NA (see note 2) C5 C6 (see note 3)
Adaptivity 5.4.9 C9
Receiver Blocking 5.4.10 C7 C8

C1, C3: The lowest declared channel for every declared Nominal Channel Bandwidth within this band.

For the Power Density testing, it is sufficient to only perform this test using the lowest Nominal

Channel Bandwidth.

C2, C4: The highest declared channel for every declared Nominal Channel Bandwidth within this band.

For the Power Density testing, it is sufficient to only perform this test using the lowest Nominal

Channel Bandwidth.

C5, C6: One channel out of the declared channels for this frequency range. If more than one Nominal

Channel Bandwidth has been declared for this sub-band, testing is performed using the lowest and highest Nominal Channel Bandwidth.

C7, C8: One channel out of the declared channels for this sub-band. For Occupied Channel Bandwidth, testing is repeated for every declared Nominal Channel Bandwidth within this sub-band.

C9: One channel (in case of single-channel testing) or a group of channels (in case of multi-channel testing) out of the declared channels.

  1. In case of more than one channel plan has been declared, testing of these specific requirements need only be performed using one of the declared channel plans.
  2. Testing is not required for Nominal Channel Bandwidths that fall completely within the frequency range 5150 MHz to 5250 MHz.
  3. Where the declared channel plan includes channels whose Nominal Channel Bandwidth falls completely or partly within the 5 600 MHz to 5 650 MHz band, the tests for the Channel Availability Check (and where implemented, for the Off-Channel CAC) are performed on one of these channels in addition to a channel within the band 5 470 MHz to 5 600 MHz or within the band 5650 MHz to 5725 MHz.