SWRA705 August   2021 AWR1243 , AWR1443 , AWR1642 , AWR1843 , AWR1843AOP , AWR2243 , AWR2944 , AWR6443 , AWR6843 , AWR6843AOP , AWRL1432 , AWRL6432 , IWR1443 , IWR1642 , IWR1843 , IWR2243 , IWR6243 , IWR6443 , IWR6843 , IWR6843AOP , IWRL6432 , IWRL6432AOP

 

  1.   Trademarks
  2. Introduction and Challenges
  3. Radome Design Elements
    1. 2.1 Understanding Dielectric Constant and Loss tangent on Radome and Antenna Design
    2. 2.2 Impedance Mismatch at Radome Boundaries
    3. 2.3 Radome Wall Thickness
    4. 2.4 Antenna to Radome Distance
  4. Typical Radome Material Examples
  5. Radome Angle Dependent Error
    1. 4.1 Rectangular Radome Angle Dependent Error
    2. 4.2 Spherical Radome Angle Dependent Error
    3. 4.3 Effect of the Angle Error in the Application
  6. Radome Design and Simulations
  7. Radome Lab Experiments
    1. 6.1 Radome Experiment – 1: Flat Plastic Radome
    2. 6.2 PTFE Material Rectangular Radome
    3. 6.3 PTFE-Based Curved Radome
  8. Additional Considerations
    1. 7.1 Antenna Calibration
    2. 7.2 Radome Near Proximity Considerations
  9. Summary
  10. Acknowledgments
  11. 10References

Antenna to Radome Distance

The optimal distance between the antenna and the internal surface of the radome helps to minimize the effects of reflections caused by the radome. These effects become minimal if the waves returned to the antenna are in phase with the transmitted waves. Equation 5 shows the optimal distance that should be between antenna and radome

Equation 5. D = n * λ 0 2

Where,

  • n: 1,2,3…
  • D: optimal distance between radome and Antenna
  • λ0: wavelength in air