SWRS205F March 2017 – December 2024 CC3120MOD
PRODUCTION DATA
Table 6-1 lists the pin descriptions of the CC3120MOD module.
If an external device drives a positive voltage to signal pads when the CC3120MOD is not powered, DC current is drawn from the other device. If the drive strength of the external device is adequate, an unintentional wake up and boot of the CC3120MOD can occur. To prevent current draw, TI recommends one of the following: