SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
For the CC32xx devices, invoking the restore to factory based on the SOP lines requires additional POR and a method to request that from the end user (see Step 5).
The following steps are required:
If the user pressed the POR during Step 3, the restore process continues and the device automatically triggers an additional hibernate-reset when finished.
While the restore to factory function is in process, the networking subsystem is in lock state.
On Step 4, detection of the SOP indication(011) is done by reading the following value: (HWREG(0x4402FC18) & 0x80)
If the user sets the SOP to 010 in Step 2, the scenario described in Step 5 will not work correctly.