SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
When creating a secure file, the file resides encrypted on the SFLASH, and any access to the secure file requires a token. The default behavior is that the open for create function returns the master token of the file, the token is kept by the host application, and is then used for the file operation (read/write/delete).
To prevent a situation in which the host application was powered off before the received token is kept, use one of the following methods: