SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Removing a filter is initiated by removing the filter from the active filters list. If a filter is persistent, removing it is not enough and the STORE operation must also be called.
In this command, filters with bits set to 1 are removed, and filters with bits set to 0 or filters which are not defined are ignored.
To remove filters, call the sl_WlanSet API with the following arguments: