SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Access point (AP) is supported by the SimpleLink Wi-Fi device. This mode is used mostly to set the device network configuration. In AP mode, the unprovisioned SimpleLink Wi-Fi device wakes up initially as an AP with an SSID defined by the equipment manufacturer. Before trying to connect to the home network for the first time, the unprovisioned device creates a network of its own, allowing a PC or a smartphone to connect to it directly and facilitate its initial configuration. AP mode supports up to four connected stations and offers a secured connection. Managing the station connection can be done by using host commands (distribute IP address, see connected stations, disconnect stations, add or remove stations from the black list, and so on). Specific settings and modes of operation are unique for AP mode.