SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
SimpleLink Wi-Fi devices support multiple internal-device configurations and settings such as device initialization, communication interface settings, time and date settings, and more, using simple host-driver commands.
In the following chapters, the word device describes the network subsystem.