SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Non-serving channels are channels that the system uses temporarily. For example, during scanning. On these channels, the device performs a fast calibration. The fast calibration is initiated by the device upon need and the calibration data is stored in the file system when sl_Stop() is called from the host interface (similar to the serving channel). The data contained in these calibration contains calibrations of all channels.
Re-calibration for the 5 GHz Wi-Fi non-serving channels will be invoked on the following cases: