SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Figure 17-7 depicts successful AP provisioning with cloud confirmation.
When feedback is provided through a cloud server (external confirmation), the host can send commands to the networking subsystem to connect to the cloud-based server only after the IP acquired event is received.
Because the networking subsystem is unaware of the results coming from the cloud server, the host is responsible for stopping the provisioning process and to order the networking subsystem to stay in its active role (STA), when confirmation is successful. For the same reason, the host must order the networking subsystem to stop the profile confirmation attempt (by sending the ABORT_EXTERNAL_CONFIRMATION command) when confirmation fails.