SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
This state is used to enable the host to run test code to decide if the downloaded bundle files are working as expected.
While in this state, opening files for read returns the content of the new files copy.
While in this state, files cannot be opened for write with the bundle flags; in such cases, the device returns an error:
SL_ERROR_FS_BUNDLE_NOT_IN_CORRECT_STATE
.
Transition from this state to the STOPPED state is executed if one of the following scenarios is fulfilled: