SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Whenever possible, the SimpleLink device strives to enter and remain in its low-power state (LPDS). In this state, most of its clocks and logic are powered down, and only the memory and basic supervision circuitry are enabled, which leads to low power consumption. The host interface is designed such that entering and exiting LPDS is completely transparent to the host. The host may initiate a new command at any time, regardless of the power state of the device.