SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
As mentioned, the calibration data is kept during a call to sl_Stop(). Giving the system the necessary time to store the data lets the system skip the calibration step if the data is still valid. This helps the overall power consumption.
800 mSec should be enough time to store the data for most use cases, but it depends on several different parameters, such as the working temperature and number of erase cycles done on the target page. The user should take into account these values, according to the exact SFLASH part that is used.