SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
When the provisioning process starts, the SimpleLink Wi-Fi device waits for the end-user to provide it (using an external tablet or smartphone app) with the information needed to connect to a wireless network:
The provided information is saved into the device serial flash memory as a new profile.