SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
The rule structure describes the match criteria. The rule is a combination of:
During the packet processing, the value of the frame field is compared with the value of the rule arguments. For example:
The structure of the rule is a union which serves two types of rules: the header rule type and the combination rule type. For rule of type SL_WLAN_RX_FILTER_HEADER, the structure used is SlWlanRxFilterRuleHeader_t.