SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Committing the bundle approves all the files which belong to the bundle. At the end of the process, all the bundle files are in the standard file state, and the bundle state is in the STOPPED state. In addition, the newly downloaded version of the files becomes the active one.
The commit process is fail-safe; that is, if the device has been shut down during the bundle commit procedure, on power-up the device automatically continues the bundle commit process.