SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Options are used to enable or disable features, or to set some configurations to the TLS socket. To change the options, use the BSD sl_SetSockOpt with unique options.
If no options were set, the following defaults take effect:
The socket settings (specified in Section 8.5.1) must be called before the sl_Connect or sl_Listen commands to take effect. In server mode, those settings are inherited by the child socket, and cannot be applied directly on the child socket.
Setting the server certificate and private key are mandatory when opening an TLS server.