SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
The programming image is a packed file which contains the service pack, the system configuration files, the user files, and the host application (in CC32xx devices ).
The process of creating the programming image is an offline process.
For creating the programming image, the SimpleLink Wi-Fi package contains the Image Creator tool, a web application (it also has CLI interface) which lets the user easily create the programming image and supports programming the device.
The UniFlash Image Creator tool creates four types of files:
The programming image can be created as encrypted (AES-CTR 128); the key used for the encryption must be supplied during the image programming.