SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Connection to a WLAN network is one of the basic capabilities of the SimpleLink Wi-Fi device, and it is the first step required before initializing socket communication. The SimpleLink Wi-Fi device supports two methods of establishing a connection: manual connection and preferred networks.
Each of the following methods is combined with a predefined connection policy which instructs the SimpleLink Wi-Fi device on how to act in different states. Indication of connection completion is provided to the application through an asynchronous event (see Section 5.3.4).