SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
A typical usage for the send event capability is to perform wake on WLAN (that is, to wake the host on a specific packet matching a filter).
Events can be sent from the SimpleLink Wi-Fi network processor to the host as a result of a matched Rx filter.
The event action arguments (Action.UserId) define the bit number set in the triggered event.
The supported ID range is from 0 to SL_RX_FILTER_MAX_USER_EVENT_ID (=63).
A single host event aggregates all the events actions which have been triggered for a single frame. The aggregation is based on the filter groups, as described in rule types. Examples follow.