SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Figure 25-12 shows the typical 5-wire UART topology which is comprised of 4 standard UART lines, plus one IRQ line from the device to the host controller to allow efficient low power mode.
This is the typical and recommended UART topology, as it gives the maximum communication reliability and flexibility between the host and the SimpleLink device.