SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
The HTTP server automatically replaces token names with their values when it serves files from the file system or ROM. For example, if a text file is created on the file system under the path /www/example.txt with the content:
Device hardware version: __SL_G_V.D
Device network version: __SL_G_V.A
Then a GET request to mysimplelink.net /example.txt returns the following text:
Device hardware version: 20000000
Device network version: 3.92.1.1
The tables in the following sections specify all supported tokens.