SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
This chapter gives a brief introduction to the networking subsystem, lists the key features of the device, and provides an overview of the host driver.
The SimpleLink™ Wi-Fi® family of devices consist on two types of devices: wireless MCU devices with a built-in network processor, and network processor standalone devices.
The SimpleLink™ Wi-Fi® CC31xx wireless network processor allows the connection of any low-cost, low-power microcontroller (MCU) to the Internet of Things (IoT), using standard communication interfaces such as SPI or UART. The scope of this document covers the following part numbers belonging to this type: CC3120, CC3130, and CC3135.
The SimpleLink™ Wi-Fi® CC32xx is a wireless MCU with an integrated high-performance Arm®Cortex®-M4 MCU, built-in Wi-Fi®, and a networking subsystem, allowing developers to write an entire application with a single-chip solution. The scope of this document covers the following part numbers belonging to this type: CC3220R, CC3220S, CC3220SF, CC3235S, CC3235SF, CC3230S, and CC3230SF.