SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
When provisioning is started in AP + SC + external configuration mode, and the user is using one of the internal provisioning methods (AP or SC), the device sends a reset request event to the host. The host should stop all of its external provisioning activities, and restart the device. Once the device is restarted, it starts the profile confirmation, and the internal provisioning process continues as usual.