SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
The SimpleLink Wi-Fi device supports three WLAN modes: STA, AP, and Wi-Fi-Direct. The device can run one mode at a time. Each mode has specific settings and capabilities which are detailed in the following sections. Using the WLAN modes, connection, scanning networks, and data transmissions are possible. This chapter describes the full set of capabilities of the WLAN system.