SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
The SimpleLink device has an internal DNS server which runs in AP mode and Wi-Fi Direct mode (GO). The DNS server is enabled by default and can be disabled. The DNS server resolves the SimpleLink device IPv4 address. The default domain name is mysimplelink and it can be configured (see Section 4.10).
Example:
_i16 Status;
Status = sl_NetAppStop(SL_NETAPP_DNS_SERVER_ID); // Stop DNS serverif( Status )
{
// error
}